Technical FAQs

Ask a Question

What affect does the %MWi Reset on Cold Start have on the %MW values in the PLC?


If %MWi Reset on Cold Start is selected those %MW's in the application having Initial Value will be populated, those %MW's not having Initial Values will be set to zero or initialized.
If %MWi Reset on Cold Start is not selected all %MW's in the application will be set to zero or initialized

 


Was this helpful?
What can we do to improve the information ?