Technical FAQs

Ask a Question

Where to locate the serial number of Sepam 60 and 80 base units?

Aside from acquiring the serial number of Sepam 60 and 80 base units via the front panel, SFT2841, or SFT SAV, it is also possible to acquire the serial number by looking at the base unit itself. Unfortunately, sometimes people get confused with the serial numbers of the other modules connected the base unit, for example the MES module and application cartridge.

For Sepam 60 and 80, the serial number of the base unit is printed on a sticker located on the front panel cover of the Sepam.


AEDL3
Was this helpful?
What can we do to improve the information ?