Technical FAQs

Ask a Question

Does Schneider Electric offer a direct replacement for IFA62/3DP0-DS/5DC-B54/2-015KZZ54 with ID number of 66206290001 ?

No, the IFA62/3DP0-DS/5DC-B54/2-015KZZ54 is an OEM specific model that has some unique features which are not offered in our standard catalog.

The IFA62/3DP0-DS/5DC-B54/2-015KZZ54 has a 15:1 gearbox which is not a standard offer
The IFA62/3DP0-DS/5DC-B54/2-015KZZ54 also has a 48 volt DC power rating as compared to the 36 volt DC power rating of our standard offer of ILA1B motors.

Customers in need of IFA62/3DP0-DS/5DC-B54/2-015KZZ54 must contact the OEM machine builder to purchase a spare.

 
Was this helpful?
What can we do to improve the information ?