Technical FAQs

Ask a Question

Osisense XM_XMPC06C2941C701 specifications and how to order in 2016

1) The XMPC06C2941C701 power switch is the "standard" XMPC06C2941 (available under logistic ref. XMPC09C2941AB in 2016, with definition of the fluid entries A, B, C & D), supplied with the C701 specification.

2) C701 specifications meaning, in the XMPC06C2941C701 reference
  • 1/2 gas fluid connection drilling in A (see attached file for fluid entries designation);
  • 1/4 gas fluid connection drilling in C;
  • B and D closed;
  • Pressure factory settings : 2.0-3.5 bar.
3) How to order the XMPC06C2941C701 reference in 2016 : it has to be ordered under the following logistic reference XMPC06C2941C701AB (internal Schneider rule); nothing to define at order. Logistic situation : available, manufactured at order reception.
XMP fonds A B C D.jpg
Was this helpful?
What can we do to improve the information ?