Technical FAQs

Ask a Question

Osisense XM_Is it possible to order the special XMPC12C2941C702 power switch in 2016?

1) Please note that the reference XMPC12C2941C702 does not exist in our technical & commercial data base, meaning it is not defined technically. The correct reference could be :
- either the XMPC12C2941S702, still available to order in 2016, under logistic reference XMPC12C2941S702AB (internal Schneider rule). Product manufactured at order reception, origin Czech Republic;
- either the obsolete XMPC12C2931C702 reference, discontinued in 1998.

2) S702 specifications meaning, in the reference XMPC12C2941S702
  • 1/2 gas fluid connection drilling in A (see attached file for fluid entries designation);
  • 1/4 gas fluid connection drilling in C;
  • No factory settings for the pressure.
XMP fonds A B C D.jpg
Was this helpful?
What can we do to improve the information ?