Technical FAQs

Ask a Question

What is included in Advantys part number STBAVO1250K?

The "K" at the end of the part number designates kit. The kit now contains the following parts:
One STBAVO1250 analog output module
One STBXBA1000 base
Two STBXTS1100 6-terminal screw type connectors
Two STBXTS2100 6-terminal spring clamp connectors
Was this helpful?
What can we do to improve the information ?