Technical FAQs

Ask a Question

Why do each of my 140CPU67160 processors indicate "Run Offline" ?

One common reason for the "Run Offline" condition is that the CPU's do not see at least one viable RIO drop.
In order to establish HSBY you must meet minimum hardware requirements.These requirements include a connection between the RIO heads (140CRP93x 00)
and at least one RIO drop (140CRA93x 00).

This minimum requirement also applies to 140CPU67160's using the 140CRP312 00 & 140CRA312 00  QERIO solution.

 
Was this helpful?
What can we do to improve the information ?