Technical FAQs

Ask a Question

Can the 140CFA04000 Cablefast block be used with the 140ATI03000 module?

The 140CFA04000 block does not incorporate an isometric barrier and is not
recommended for use with the 140ATI03000 TC module. Without such a barrier,
temperature readings may vary up to 2 degrees from one end of the block to the
other. If the application can tolerate this temperature error, the block (and module
remote CJC) may be used.
Was this helpful?
What can we do to improve the information ?