Technical FAQs

Ask a Question

What is the suggested replacement for the Magelis XBTE?

Issue:
What is the suggested replacement for the Magelis XBTE?

Product Line:
XBTE013010, XBTE013110, XBTE014010, XBTE014110, XBTE015010, XBTE016010, XBTE015110, XBTE016110, XBTE016010M167


Environment:


Cause:


Resolution:
The suggested replacement for the XBTE is HMIGK2310.  HMIGK2310 is due to be release in 2017.  Keep in mind that XBTE project can not be converted over to the HMIGK2310.  It does require a reprogramming of the application to the new replacement with a different programming software package.
Was this helpful?
What can we do to improve the information ?