Technical FAQs

Ask a Question

What are specifications of the fiber optic cable bearing part number 990MCO000xxx:?

   It is a SERCOS SMA 1000-micron plastic fiber optic cable

- Diameter - 1mm plastic fibre
- Radius of curvature: >= 0.98 in (25 mm)
- The core's diameter in microns: 1000 (1mm).
- connector type: SMA
- Operating temperature range: between -40 °C and 80 °
- Maximum traction effort during installation: 25 kg/cab
Was this helpful?
What can we do to improve the information ?