Technical FAQs

Ask a Question

Video: Creating a 984LL segment section in Unity Pro?

After opening a new Unity Pro project and a PLC has been selected, follow these steps to create a new 984LL Segment Section:
  • In the Project Browser under Program >> MAST create a New Section and choose the 984LL . The new section appears under sections.
  • Click and open the new section and create a 984LL segment
  • Click OK
  • Confirm the 984LL editor appears on the screen.


Was this helpful?
What can we do to improve the information ?