Technical FAQs

Ask a Question

Video: How can the installation of Unity Hotfixes be verified?

To verify Hotfixes are installed in Unity Pro, use the following procedure:
  • From any window in Unity ( preferably the main screen ). Point and click Help, and select “About Unity Pro “.
  • When the “ About Unity Pro “ window appears point and click on “ Technical Info “.
  • All installed Hotfixes will be listed. OK or X to exit.
The following video demonstrates this procedure.

Was this helpful?
What can we do to improve the information ?