Technical FAQs

Ask a Question

What would cause ProWORX 32 ERR=75 Path/File access error?

The ProWORX 32 "Path File Access" error usually has to do with Administrator rights on the PC. You should have full administrator rights on the PC and log on as Administrator. This will clear the "Path File Access" error.
Was this helpful?
What can we do to improve the information ?