Technical FAQs

Ask a Question

Video: How to configure the ProWORX 32 network logic view screen

Follow this procedure for configuring the ProWORX 32 network logic view screen:
1- Open the project Properties window. Go to PROJECT > PROPERTIES.
2- Select the LOGIC tab.
3- Configure the Logic window to show:
     Descriptor1 > select the color Green
     Symbol1 > select the color Red
     Address > automatically preset for Black
     Data > select the color Blue
4- Click the APPLY and OK buttons to save the settings.
5- Your network logic screen will now display the selected options with the coordinated colors.

 
Was this helpful?
What can we do to improve the information ?