Technical FAQs

Ask a Question

Osisense XC - Cross-reference of the special XCMA1436439 limit switch with ball bearing roller plunger

The special XCMA1436439 limit switch, discontinued in 2006, was a special XCMA117* with a M12 4-pin connector on a pig-tail. It is replaced by the equivalent XCMD1436439 limit switch, manufactured at order reception (see attached description). Sales open to all customers.
Was this helpful?
What can we do to improve the information ?