Technical FAQs

Ask a Question

Is Unity Pro compatible with Windows 10 O.S.?

Yes. Unity Pro v11 & v11.1 is supported on the following Windows Operating Systems:

> Windows 7 32&64 bits
> Windows 8.1 32&64 bits
> Windows 10 32&64 bits
> Windows Server 2012

 
Was this helpful?
What can we do to improve the information ?