Technical FAQs

Ask a Question

Osisense XC - Cross-reference of the special XCMA1423381 limit switch with steel roller plunger

The special XCMA1423381 limit switch, discontinued in 2005, was a standard XCMA102 (see attached picture) with a specific cable lenght of 5.6 metre. It is replaced by the equivalent XCMD1423381 limit switch, manufactured at order reception.
Was this helpful?
What can we do to improve the information ?