Technical FAQs

Ask a Question

Osisense XC - Cross-reference of the special XCMA1656046 limit switch with steel roller plunger and a 5-pin M12 connector

The special XCMA1656046 limit switch, discontinued in 2005, was a standard XCMA102T200 (see attached picture) with a specific M12 5-pin connector (special wiring with internal jumper). It is replaced by the equivalent XCMD1656046 limit switch. It is in stock in our international distribution centre.
Was this helpful?
What can we do to improve the information ?