Technical FAQs

Ask a Question

Osisense XC - Cross-reference of the special XCMA1656047 limit switch with metal end plunger and a 5-pin M12 connector

The special XCMA1656047 limit switch, discontinued in 2005, was a standard XCMA110T200 (see attached picture) with a specific M12 5-pin connector (special wiring with internal jumper). It is replaced by the equivalent XCMD1656047 limit switch. It is produced at order reception in the production plant.
Was this helpful?
What can we do to improve the information ?