Technical FAQs

Ask a Question

What Operating System are supported with SCADA Expert ClearSCADA 2015 R1 ?

 Refer to the following table for supported Operating System versions  for SCADA Expert ClearSCADA 2015 R1 ?:

  32-Bit 64-Bit
Desktop Hardware Windows 8.1 (Professional edition)
Windows 8 (Professional edition)
Windows 7 Service Pack 1 (Professional and Ultimate editions)
Windows 8.1 (Professional edition)
Windows 8 (Professional edition)
Windows 7 Service Pack 1 (Professional and Ultimate editions)
Server Hardware Nil Windows Server 2012 R2 (Standard and Datacenter editions)
Windows Server 2012 (Standard and Datacenter editions)
Windows Server 2008 R2 Service Pack 1 (Standard and Enterprise editions)
Was this helpful?
What can we do to improve the information ?