Technical FAQs

Ask a Question

Scadapack RTU cannot write to Wago RTU over modbusTCP ?

To solve issue its necessary to know following things and set them correctly in MTCP_INT_WRITE IOdevice in scadapack workbench.
-The correct memory address for holding registers should be set in IOdevice to be read and written. Wago RTU has specific zones of modbus register which can be read and written.
-Modbus address format to be used by modbus master MTCP_INT_WRITE IOdevice should  '6' digit to write to Wago.  Wago RTU address which contains value is mapped at 6 digit modbus register location.
-Unit ID must be set correctly as defined in Wago RTU..
Setting all above things correctly as shown below solves issue.
Was this helpful?
What can we do to improve the information ?