Technical FAQs

Ask a Question

Osisense XC - Cross-reference of the special XCMB1656081 limit switch with steel roller plunger

The special XCMB1656081 limit switch, discontinued in 2005, was a standard XCMB502 (see attached picture) with a specific M12 5-pin connector (special wiring). It is replaced by the equivalent XCMD1656081 limit switch, manufactured at order reception.
Was this helpful?
What can we do to improve the information ?