Technical FAQs

Ask a Question

Osisense XC - Cross-reference of the special XCKP438298001 limit switch with plastic roller lever

XCKP438298001 in black plastic casing, discontinued in 2005, was an obsolete XCKP118 limit switch (see attached picture), supplied with all the metallic parts in stainless steel : roller lever, roller axis, head screws, nut plate ... It is replaced by the equivalent XCKN438298001 switch, in blue plastic casing. Sales are open for all customers and it is in stock in our international distribution centre. Sold by quantity of 20 pieces.
Was this helpful?
What can we do to improve the information ?