Technical FAQs

Ask a Question

Osisense XC - Cross-reference of the special XCKP415979 limit switch with plastic roller lever

XCKP415979 in black plastic casing, discontinued in 2005, was an obsolete XCKP518 limit switch having a plastic Pg11 cable gland mounted in the body. Attached picture of the obsolete switch, without the cable gland. It is replaced by the equivalent XCKN415979 switch, in blue plastic casing. Sales are open for all customers and it is in stock in our international distribution centre. Sold by quantity of 20 pieces.
Was this helpful?
What can we do to improve the information ?