Technical FAQs

Ask a Question

Osisense XC - Cross-reference of the special XCKP1305554 limit switch with plastic roller lever

Attached picture of the obsolete XCKP1305554 in black plastic casing, discontinued in 2005.
It is replaced by the equivalent XCKN1305554 switch, blue plastic casing, having the same roller lever. Technically it is a standard XCKN2118G11 switch with a special roller lever (roller dia 19mm, 12mm large). The roller lever is not mounted at product delivery. Sold by quantity of 1.

Dimensions in mm
Was this helpful?
What can we do to improve the information ?