Technical FAQs

Ask a Question

We do not understand why the userguige state default a transfer passcode"5.6.5.6", because we could use eXLhoist without transfer passcode.

The code "5.6.5.6" given for the transfer password it a mistake, actually in the factory setting there is no transfer password."
Was this helpful?
What can we do to improve the information ?