Technical FAQs

Ask a Question

Osisense XU - Factory settings of the XUK9TAH2MM12 laser sensor "Time of Flight" for anticollision function

The factory settings of the XUK9TAH2MM12 laser sensor  "Time of Flight" for anticollision function, are the following
QA : 4 mA = 0,3 m / 20 mA = 70 m
Q1 : 2 ... 6 m
Q2 : 2 ... 6 m
Was this helpful?
What can we do to improve the information ?