Technical FAQs

Ask a Question

SPM/PME - Diagnostic Tool Failure & Issue editing/adding Data Series and with measurement groups in Dashboards

Issue
Attempting to Edit or Add to the Data Series for an existing gadget will present and 'Error loading measurements' message. The diagnostic tool fails to archive any of the ION_Data, ION_Network and Application Modules databases. The error below is observed in the Windows Application Event Log.
Source = MSSQL$STXPWRMON
General tab = The description for Event ID 17053 from source MSSQL$STXPWRMON cannot be found. Either the component that raises this event is not installed on your local computer or the installation is corrupted. You can install or repair the component on the local computer.

Product Line
StruxureWare Power Monitoring Expert

Environment
StruxureWare Power Monitoring 7, Power Monitoring Expert 7.2, Power Monitoring Expert 8, SQL Server 2008 R2, SQL Server 2012, SQL Server 2014


Cause
The 'tempdb' (temprorary database) is running out of disk space and thus is interfering with PME operations such as retreiving topics for dashboards. The databases archive fails as the diagnostic tool attempts to use 'tempdb' as part of the process.

The following information is included with the event.


D:\Program Files\Microsoft SQL Server\MSSQL10_50.STXPWRMON\MSSQL\DATA\templog.ldf
112(There is not enough space on the disk.)


Resolution
- Run the Windows Disk cleanup tool to free up disk space and delete temprorary files.

Because tempdb is re-created each time the instance of SQL Server is started, you do not have to physically move the data and log files. The files are created in the new location when the service is restarted. Move the 'tempdb' database and log files to another location by following the steps in KB FA219030.
 
Was this helpful?
What can we do to improve the information ?