Technical FAQs

Ask a Question

Preventa XCS - Is it possible to install the XCSDMP magnetic switch on an aluminium support without reduction of the nominal Sao and Sar?

Please note that some materials are non-magnetic or paramagnetic ones, i.e. not attracted by a magnet or an electric field (non-ferrous materials): glass, aluminum, lead, copper, brass, some stainless steels, plastic ... To check that some aluminium alloy or material is non-magnetic, you have to check it by a regular magnet : if it does stay on the support, it means it is non-magnetic. So no performance reduction for the Sa0 and Sar distances.
Was this helpful?
What can we do to improve the information ?