Technical FAQs

Ask a Question

How to reach modbusplus network devices from modbus native port of quantum CPU 140CPU67160 ?

As an example to demonstrate to read modbusplus nodes from serial modbus port  just see an architecture to test bridge mode with quantum HSBY PLC.
Mb+ Node address of Primary PLC is ‘1 ‘  and Standby is ‘33’ as default.



By enabling Bridge Mode in CPU configuration , the modbus master request is bridged and routed to modbusplus devices on MB+ network. Also correctly set serial communication parameter.

For example master is connected to modbus port of primary CPU, modbus master can read from both the devices with Mb+ addresses 1 and 33 as modbus addresses or can access any other node over modbusplus. This is advantage of bridge mode.
Was this helpful?
What can we do to improve the information ?