Technical FAQs

Ask a Question

What are the Modbus Requests/PLC Scan Cycle, number of simultaneous TCP/IP connections (sockets) in Client/Server mode for MC80 PLC

In MC80, Modbus server will process 8 requests per cycle.Simultaneous TCP/IP connections for client is 4, for server is 16.

 
Was this helpful?
What can we do to improve the information ?