Technical FAQs

Ask a Question

What is included in TSX Micro series part number TSX37210PAK10?

TSX37210PAK10 is obsolete and no longer available. It was comprised of the following parts:
TSX3721001.....TSX Micro modular base controller
TSXETZ510.....Ethernet TCP/IP module
TSXMRPC448K.....SRAM memory card

These parts are still available as individual purchase items.
Was this helpful?
What can we do to improve the information ?