Technical FAQs

Ask a Question

What is the replacement part number for a Berger Lahr IFS93/2DP0-DS/3DI-B54/3-005KPP54 with ID number 66109300022 ?

Schneider Electric offers this motor as a current product.
However, the motor, gearbox and gearbox mounting kit are ordered as separate line items.

Below are the three part numbers used for ordering.

ILS1B853TB1A0  = motor IFS93/2DP0-DS/3DI-B54/ without gearbox
GBX080005K  = gearbox  5:1
GBK080853S  = gearbox mounting kit

All three items can be ordered or only those items which are needed.
Was this helpful?
What can we do to improve the information ?