Technical FAQs

Ask a Question

What is the factory default IP address for Ethernet based Trio Radios ?

The factory default IP address  is 192.168.2.15. If you do not know the IP address then you will need to activate a factory reset. 
Was this helpful?
What can we do to improve the information ?