Technical FAQs

Ask a Question

How to force ION7550/7650 out of Test Mode?

ION7550/7650 will not exit Test Mode even after the messsage "Meter is now back in normal mode" appears in ION Setup.

Product Line

ION Setup

Test Mode is still Enabled

To force the meter out of Test Mode:
  1. Enter into Advanced ION Setup by holding the Ctrl key and clicking on the meter. The Modules should then populate the right side of the screen as shown.
  1. Select Ext Bool Modules in the left panel.
  1. Then double-click the Test Mode Enble module
  2. The output register Test Mode Enble controls whether the meter is in Test Setup.
  1. By holding the Shift key and clicking on the paramter, you can toggle the Test Mode Enble value between OFF and ON. To force the meter out of Test Mode, turn the enable OFF. The meter should now be in Normal Mode.
Was this helpful?
What can we do to improve the information ?