Technical FAQs

Ask a Question

Osisense XU_Reliability data of the XUK8TAKSMM12 laser transmission sensor MTTF?

The reliability data of the XUK8TAKSMM12 laser transmission sensor, with background suppression and time of flight, are the following :
- MTTF = 166.5 years (mean time to failure),
- MTTFd = 333 years (mean time to dangerous failure),
- DC = 0 (diagnostic coverage) of the sensor alone,
- mission time = 20 years.
They are used for the functional safety, according to the ISO 13849-1 standard (Performance Level).
The MTTF calculation is made according to the EN/IEC 61709 standard (SN 29500).
Was this helpful?
What can we do to improve the information ?