Technical FAQs

Ask a Question

Osisense XC special - XF9HB3211 type of reset

It is the last digit of the complete XF9 reference, which defines the resetting type of the XF9F/H/G power switch for overtravel control.
  • XF9****1  manual latching and reset  (your XF9HB3211 reference)
  • XF9****2  with counterweights and automatic reset
Was this helpful?
What can we do to improve the information ?