Technical FAQs

Ask a Question

Latest firmware version for the energy server COM'X 510 (Version 3.5.24)

Issue
What is the latest firmware version for the Energy Server Com'X 510 ?
 
Product Line
COM'X 510
EBX 510
 
Resolution
As of 12/20/2016, the latest version of firmware for COM'X 510 is 3.5.24, which is available to download from the link below:
http://www.schneider-electric.com/en/download/document/ComX510v3-5-24_Firmware_EBX510/


Instructions for upgrading the firmware can be found from KB FA270261
Was this helpful?
What can we do to improve the information ?