Technical FAQs

Ask a Question

How come when I input the IP address of the HMIDT643, it is taking me to the WLAN settings and not Web Gate?

Issue:
How come when I input the IP address of the HMIDT643, it is taking me to the WLAN settings and not Web Gate?

Product Line:
HMIDT643, HMIG5U, access point, WLAN, Web Gate, webgate

Environment:


Cause:


Resolution:
If you set up the WLAN of the HMIDT643 as an Access Point.  You need to assign a static IP address to the Local Area Connection of “LAN9500A USB 2.0 to Ethernet 10/100 Adapter”.  This will allow the Web Gate connection on the WLAN adapter.
Was this helpful?
What can we do to improve the information ?