Technical FAQs

Ask a Question

What is the permissible ambient operating temperature for Lexium SD328 drives?

The Lexium SD328 is rated for ambient temperature range of 0c - +40c per UL listing.
The drive may be operated in ambient conditions ranging from 0c - +50c if operated at reduced output current. 
Current reduction should be 2.2% for each degree above 40c

 
Was this helpful?
What can we do to improve the information ?