Technical FAQs

Ask a Question

Concept function blocks that are not included in a Concept to Unity conversion.


Yes, and in addition to the following list you can also include SCALRTOW and SCALWTOR..


  PLCSTAT and READREG will come into Unity as a DFB. These can be added to the Library which will allow these blocks to be use on all subsequent applications.

 


Legacy KB System (APS) Data: RESL211858 V1.0, Originally authored by DaSo on 06/21/2013, Last Edited by DaSo on 06/21/2013
Related ranges: Unity Pro - SoCollaborative software


R-6-30-17
Was this helpful?
What can we do to improve the information ?