Technical FAQs

Ask a Question

Where can I find the part numbers and pricing for the Automation support program?

The Automation Support Program allows the customer to have priority telephone support as well as keep their software up to date.  The Automation Support Brochure goes over the different levels of support offered at our Andover, MA Support Center.  The Automation Support Pricing Brochure has a grid that will provide the part numbers and pricing based on the type of software platforms you have as well as the number of licenses.   If you still have questions don't hesitate to contact the Contract Support Group at 888-266-8705 option 3.
Was this helpful?
What can we do to improve the information ?