Technical FAQs

Ask a Question

Does Unity Dif run in a virtual environment?

Unity DIF is a comparison software that compares the Unity Pro project files and displays the differences graphically.
The result of the comparison is displayed in the Unity DIF main window, which can be printed/saved as .pdf or .txt format.

The software compares the project files with .xef, .zef, .stu, and .sta

Unity DIF on a Virtual Machine
Unity DIF runs on the following virtual machines:
  • VMWare
  • VirtualBox
VMWare
VMWare requires the given configurations:
Operating System of VMware machine Operating System of Computer
Windows 7 (64 bit) Windows 7 (64 bit)
Optional Configurations
Windows 7 (32 bit) Windows 7 (32 bit)
Windows XP Windows 7 (64 bit)
 
VirtualBox
VirtualBox requires the given configurations:
Operating System of VirtualBox machine Operating System of Computer
Windows 7 (32 bit) Windows 7 (64 bit) (recommended) Or Windows 7 (32 bit)
Was this helpful?
What can we do to improve the information ?