Technical FAQs

Ask a Question

What is the tapping range alternatives of the OLTC of the Minera SGrid ODT Transformer?

We offer two alternative tapping range; one with five tappings (±2 x 2,5%, in total 5 steps) and the other with nine tappings (±4 x 2,5%, in total 9 steps).
Was this helpful?
What can we do to improve the information ?