Technical FAQs

Ask a Question

What is the power rating limit of Minera SGrid ODT transformer?

The Minera SGrid ODT transformer is designed for power ratings max 1000kVA with primary voltage up to 36kV. Higher power ratings in the application field is not a practical application and general requirement.  The demand is going around for 1000kVA and  below power ratings. The most popular power ratings for this application is 250kVA, 400kVA and 630kVA.
Was this helpful?
What can we do to improve the information ?