Technical FAQs

Ask a Question

Osisense XC - XCMB1587694 replacement

The special XCMB1587694 limit switch is a switch based on the obsolete XCMB limit switch (slow break contacts), discontinued in 2005. This special is not replaced in the XCMD range launched in 2004. Attached technical information about such switch. It does not have any cable or connector on pig-tail. Alternative for replacement is to use the sandard XCMD switch having 2 contacts slow break like the XCMD2510L1 switch, and add a M12-4 pin connector on a short length pig-tail to adapt to the existing M12 cabling. Note that the XCMD2510M12 switch does not exist in slow break, only in snap action XCMD2110M12.
Was this helpful?
What can we do to improve the information ?