Technical FAQs

Ask a Question

What is the Schneider Electric replacement number for a Berger Lahr VRDM3910/50 LWB motor with ID number 52626036000 ?

The exact replacement for the Berger Lahr VRDM3910/50 LWB type motor with ID number 52626036000 is the Schneider Electric ordering number BRS39AW260ABA

However, it should be noted that BRS39AW260ABA has never been sold in North America and this part number is not offered by Schneider Electric in North America.
This is due to the fact that this motor has a unique shaft option of a 9.5 mm smooth shaft.

Customers in North America looking for BRS39AW260ABA should substitute with the part number of BRS39AW560ABA.
BRS39AW560ABA is the same motor except it comes with a 9.5mm keyed shaft.  The keyway can be removed thereby allowing customers to use BRS39AW560ABA as a suitable substitute.

In summary the Berger Lahr VRDM3910/50 LWB type motor with ID number 52626036000 "exact" replacement is BRS39AW260ABA, but because this model is not offered in North America you should use BRS39AW560ABA as a replacement and simply remove the keyway from the shaft.

 
Was this helpful?
What can we do to improve the information ?