Technical FAQs

Ask a Question

How to Use the BMEAHI0821 and BMEAHO0412 with Quantum

Goals and Symptoms
What QNOC to use?
Facts and Changes
BMEAHI0821, BMEAHO0412, 140NOC78000
Causes and Fixes
Following the DMDI 3093E announcing the support of X80 HART modules BME AHI 0812 and BMEAHO 0412 in X80 drops behind  QUANTUM, the right modules, firmware and software to use are:
  • Unity Pro V10 + update Unity UnityPro_V100_HF0300848R
  • 140NOC78000  firmware version 1.67
  • BME AHI 0812, BME AHO 0412   firmware version 1.1
Was this helpful?
What can we do to improve the information ?