Technical FAQs

Ask a Question

What is Power Launcher, and where can I download it?

Issue

Customer has requested information on Power Launcher software, and is interested to downloading it.

Product Line

Power Launcher software

Resolution

As of March 2015, Power Launcher is no longer supported or available for download.

Here is information on the software:

Power launcher, software application that makes it easy

  • To promote the available Customer Engineering Software  in association with the following product-lines :
     - RCU/RSU  Masterpact and Compact NSX circuit-breakers
     - Acti9 Smart Test for Acti9 Smart Link products
     - ION setup for ION, PM Power meters and CM circuit-monitor
     - Powersuite for TeSys U  motors-starters and TeSys T protection relays
     - SFT software series and CET850 for  Sepam protection relays
  • To inform customers of the available software updates and to download them with a single click.
  • To customize and streamline the user experience, by enabling user «Favorites» creation
Was this helpful?
What can we do to improve the information ?