Technical FAQs

Ask a Question

Does Lexium SD326 support 5 volt or 24 volt logical signals?

Lexium SD326 support both 5 volt and 24 volt logical signal inputs.

The inputs to the Lexium SD326 are accessed via a molex socket on the face of SD326 which has 24 pins.
12 of these pins are for 5 volt signals the remaining 12 pins are for 24 volt signals.
It is the optional signal cable that you purchase that determines which pins you interface with. 

Below is a list of the accessory signal cables for SD326

  .5 meter long 5 volt cable ordering number VW3S8201R05
1.5 meter long 5 volt cable ordering number VW3S8201R15
3.0 meter long 5 volt cable ordering number VW3S8201R30
5.0 meter long 5 volt cable ordering number VW3S8201R50
 
  .5 meter long 24 volt cable ordering number VW3S8202R05
1.5 meter long 24 volt cable ordering number VW3S8202R15
3.0 meter long 24 volt cable ordering number VW3S8202R30
5.0 meter long 24 volt cable ordering number VW3S8202R50
 
Was this helpful?
What can we do to improve the information ?